This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV341A: phase reversal

Part Number: TLV341A


Does the OpAmp exhibit phase reversal when the input signal is between (V+ -0.6V) and V+ ? (unity gain configuration)

  • Marcel,

    One of two things could happen when input is greater than actual common mode range. 

    1. Output could jump up to VOH, output full high 
    2. Output could go to "actual common mode voltage" and go no higher 

    The outcome for each sample amplifier will be random but not a 50/50 chance. 
    Once the input voltage gets back into range, normal operation resumes.