Other Parts Discussed in Thread: TINA-TI
I am assigned a project about making a noise filter, amplifier which are applying the signal from photo diode.
I want to use OPA657 so i downloaded the file(OLB, lib) at here site.
and i added the OLB files correctly, and added the lib file at the 'configuration files' as global.
but there is a error message. what is the problem? i use 17.2 cadence lite version.
-----------------------------------------------------------------------------------------
*Libraries:
* Profile Libraries :
* Local Libraries :
* From [PSPICE NETLIST] section of C:\Users\travis\AppData\Roaming\SPB_Data\cdssetup\OrCAD_PSpice\17.2.0\PSpice.ini file:
.lib "C:\Cadence\SPB_17.2\userlibrary\OPA657.lib"
*Analysis directives:
.TRAN 0 1s 0
.OPTIONS ADVCONV
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*))
.INC "..\SCHEMATIC1.net"
**** INCLUDING SCHEMATIC1.net ****
* source SUMMERPROJECT
X_U1 VEE VCC N00613 0 N01062 OPA657
R_R1 0 N00613 1G TC=0,0
C_C1 0 N00613 100P TC=0,0
I_I1 N00613 0 DC 50u
V_V1 VCC 0 5
V_V2 VEE 0 -5
R_R2 N00613 N01062 200K TC=0,0
C_C2 N00613 N01062 0.1P TC=0,0
**** RESUMING TEST.cir ****
.END
ERROR -- EVALUATION VERSION analog Node Limit (75 Nodes) Exceeded!
---------------------------------------------------------------------------------------
because of the word " 75 nodes exceeded", i designed it samely at university pc room where has pspice license(not lite version)
but it did not show me the simulation result, just a gray screen even no error message.