This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rui,
Does the circuit have input pins or output pin(s) tied directly (resistance zero) to low impedance nodes. If yes, try adding a [1k, 100 ohms] resistor between device pin and the printed circuit board. de-solder and lift the pin to make space. Then try the surge test with the modification.
If you can curve trace a broken device, see which pin(s) was damaged, add more protection on that pin.