This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA169: I want to measure 3 phase motor phase with shunt and the ina169.

Part Number: INA169
Other Parts Discussed in Thread: INA240

A brushless DC electric motor (BLDC motor or BL motor), also known as electronically commutated motor (ECM or EC motor) and synchronous DC motors, are synchronous motors powered by direct current (DC) electricity via an inverter or switching power supply which produces electricity in the form of alternating current (AC) to drive each phase of the motor via a closed loop controller.

So I just want to measure the positive current of each phase for the BLDC motor[total 3 phases], so I tried to simulate it with the INA169 in software TINA.
I just cant get a good configuration , DC configuration works fine. BUT INVERTERING voltage makes it harder. The shunt resistor should measure till 7A.

I hope to hear from someone with instructions/solutions.