For a design that has two or more INA231 devices, can the ALERT pin share the same GPIO into microprocessor, assuming the ALERT is configured for normally active low and has a common pull-up resistor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For a design that has two or more INA231 devices, can the ALERT pin share the same GPIO into microprocessor, assuming the ALERT is configured for normally active low and has a common pull-up resistor?
Hello 6319281,
Thank you for considering to use Texas Instruments. The INA231 ALERT pin is connected to the drain of a mosfet. When the device is powered and the alert is not triggered, the gate voltage is below the threshold voltage, thereby making the path from ALERT to device GND look like a very large resistor. As such, having the INA231 ALERT pin share a common pull-up with other INA231s should not damage the device. The device that is triggered will pull low and the majority of current will flow from the pull-up through the triggered device. As long as the pull-up is sized such that no more than 5mA enter the ALERT pin, the device will be fine. The only problem I see with a shared pull-up would be quickly determining which device was triggered. If all devices are sharing the same pull-up and gpio, you would need to read from each device until you find the one that had been triggered.