This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4192: Question about using OPA 4192 as voltage follower (Buffer Circuit)

Part Number: OPA4192
Other Parts Discussed in Thread: TLC2274, , OPA2192, OPA192

HI, I am going to use OPA4192 as voltage follower, buffer circuit. I used TLC2274 before.

.

I will connect 

IN + : ADC Input

IN- : Connect to OUTPUT.

.

And here is my question.

When I used TLC2274, I didn't put any isolation resistor in the output. 

TLC2274 has High cload drive feature but OPA4192 doesn't have. I found High cload feature doesn't need any isolation resistor.

Then, If I use OPA4192 as buffer, then do I need isolation resistor and any capacitor? 
If I need, then how can I calculate value? 

And If priced doesn't matter then, can OPA4192 replace TLC2274 without any disadavtages as using voltage follower circuit? High Cload?  (Unity gain, buffer)

( From the datasheet OPA4192 is much better then TLC2274 in all specs. (BW, Slew rate, low offset voltage), and I think there is no reason to use TLC4192, because OPA4192 is much better. )

And OPA4192 is CMOS OP AMP?

Thanks.