Other Parts Discussed in Thread: INA293, INA190, INA186
Hi all,
I use INA293 to measure low current (10uA) with high voltage (max 100V).
Without load I see 40uA of consumption from the power supply and also some mV on the output voltage (400mV). I think the problem is the "Input bias current" on the pin IB+ and IB-.
There are some current shunt with low input bias current with high voltage (100V).
Thank you for your support
F. Buonomo