This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1200: AMC1200 incorrect schematic

Part Number: AMC1200
Other Parts Discussed in Thread: REF1933,

Hi all,

I want to measure fan speed using AMC1200BDWVR and OPA320AIDBVR. I am generating supply for ICs from TLV76050 and REF1933. However during testing, even with  AMC input open, TLV76050 was failed. Looking over the schematic I noticed that decoupling capacitor for AMC (C23, C24) we used is 100nF, 0603 package, instead of 100nF,1206 package (as suggested in datasheet). Can it be the cause of failure or anything else is creating problem? Attached are the related schematic images.

   

Thanks,

HS