Hi,
TLV27L1 datasheet states:
Abs. max rating of input voltage is Vs (Note 1 says "relative to GND pin"). is this referring to the max positive voltage allowed on the input pin?
What is the abs. max rating for the negative voltage allowed on the input pin?
Note that input common mode voltage operating condition is -0.2V. So, one would imagine that abs. max. negative voltage on input pin (relative to GND pin, or the negative supply connection) would be more negative than -0.2V.
Can TI please clarify this?
Kind regards,
Nitish Agrawal