We are looking to develop a precharge circuit in which we require to measure voltage for which we are scaling 0-500V to 0-5/10V. In this paricular component we get an output ehich can be given to an ADC. In a particular application when the output was fed into a precision amplifier. So the couple of questions which rose were is the voltage the same as input voltage ie 0-12V which is the voltage across the R2 resistor in the above diagram or does it correspond to the voltage on the output side which can be -0.3 to 6.8V and the other question is as all the parameters are given for AC voltage can this component be used for DC application.Also assuming the output is fed into ADC is the output analog