Part Number: VCA821
Hello,
I think there is something wrong in the picture of datasheet, Is there someone who have succeed simulating the circuit of this picture? I simulated this circuit with Multisim,but can't achieve the function of AGC.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: VCA821
Hello,
I think there is something wrong in the picture of datasheet, Is there someone who have succeed simulating the circuit of this picture? I simulated this circuit with Multisim,but can't achieve the function of AGC.
Hi Wen,
can you share your simulation file?
Kai
Hello Kai,
Thank you very much!
When I change the input of this circuit, the gain of the system has never changed. So I think maybe there is anything wrong.
Follow is my files, one is the simulation file of Multisim, the other is its picture.
Yours sincerely,
Wen
Hello Wen,
Would you be able to provide a screenshot of your transient simulation & labeling the issue? Can help you get this working on TINA or Pspice.
I've attached the circuit in TINA below:
Also you may want to take a look at this thread:
https://e2e.ti.com/support/amplifiers/f/14/t/152121?VCA820-Simulation-does-not-match-real-world-results
Best,
Hasan Babiker
Your original sim Hasan using 1kHz was kind of in the bandwidth of the integrator, if you need to handle really slow signals, that integrator pole needs to be really low - here is your ckt with 1MHz input, The red curve is the control voltage, the green the output signal, Looks like it is working to me.
Thanks Michael, it seems I wasn't allowing enough time in the transient sims to see this correction properly.
Best,
Hasan Babiker
Or, you should have let R8 be 100k and extend the run time to capture to a final Vg value. The Vg was moving with the 1kHz signal which is why the waveform looked so bad.