Part Number: OPA2365-Q1
Other Parts Discussed in Thread: OPA2365, AMC1301
Can I know the recommended feedback resistor value range that can be used in OPA2365 for a speed critical application.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2365-Q1
Other Parts Discussed in Thread: OPA2365, AMC1301
Can I know the recommended feedback resistor value range that can be used in OPA2365 for a speed critical application.
Hi Michael,
The desired gain is around 2. Input is a sinusoid of 1.076 Vpk and output desired is 2.052 Vpk. Can we use the feedback resistor in the 1kohm range for OPA2365 or higher than 10kohm is recommended?
Thank you in advance.
Non-inverting or inverting, what supplies and max frequency
How are you going to center up the output swing and/or stay out of clipping.
Please find the circuit configuration. Vin is a sinusoidal differential input of +/-1.076V, 2kHz. A level shift of 2.5V is added to match the ADC range. 5V supply voltage is given to the OpAmp. According to the transfer function, the ratio of R3707 to R3704 is around 2. What is the recommended range for R3707 feedback resistance.
Thank you.
Your file or picture did not come through, you need to insert those using the paperclip symbol at the top ribbon,
Please find the circuit below and the specifications as mentioned earlier. Can you please let me know the range of feedback resistor value, as it isn't mentioned in the datasheet.
Thank you in advance.
This zero crossover device (which you do not need in your app) has a fairly high input capacitance. It would be better to use 1kohm feedback (500ohm input) resistor to keep the effect of the feedback pole out of the LG phase margin.
Hi Rupali,
what exactly (in terms of R, L, C) is connected to the output of your differential amplifier? And what exactly is driving the inputs?
Kai
Hi Kai,
The output of the amplifier is going to the ADC after a RC filter of 1k, 4.7nF. The input is the output of another Isolated Amplifier, that amplifies a sinusoidal voltage signal.
Rupali
Hi Rupali,
I ask myself why you want to take such a fast OPAMP, if you have a charge kick back filter (1k / 4n7) with a corner frequency of
1Hz / 2 / pi / 1k / 4n7 = 34kHz
at its output. In this case a somewhat slower OPAmp would suffice.
Another issue is the input impedance of this circuit. This mainly depends on the isolation amplifier and how much current it can drive. What isolation amplifier are you using?
Kai
Hi Kai,
We will look into the requirement for high-speed OpAmp. And we are using AMC1301 isolation amplifier at the input side.
Rupali