Part Number: TLV3494
Hi,
I am using TLV3494, quad comparator.
Input ranges from -2.5V to +2.5V and I want the output to be 3.3V(High)- GND(Low).
I designed the supply voltage V+= 3.3V, V- = GND but input range is limited by the supply voltage.(V+ +0.5V to V- - 0.5V)
When I apply input signal from the signal generator, negative range was clamped around -1V.
Is there any possible way to solve this problem?
Best,
Jaehoon