This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM158: Alternative in SMT / SOIC 8

Part Number: LM158
Other Parts Discussed in Thread: TLV2172

Hi Team,

I have a question on LM158H/NOPB. Could you suggest me the component with same functionalities of LM158H but SMT / SOIC-8 package?

Some features have higher priorities :

  • single supply voltage +32 VDC
  • low stand-by consumption (low Iq)
  • slew rate 0.5V/us
  • temperature -40°C/125°C
  • good EMC
  • short circuit protection 

Thank you in advance,
Riccardo