Other Parts Discussed in Thread: OPA1637, OPA1611
Well I was trying to start a fresh thread on the audio forum with Iwata-san, but apparently the THS4561 forces it to the amplifier forum
Anyway, Iwata and I have been iterating on the relative merits of the OPA1637 vs the THS451 as an Audio DAC output transimpedance stage. He had noticed the higher 1/f on the current noise on the THS4561 really impacted the low frequency spot noise, and it does.
He had used the 2018 original RTM model, I found there is a 2020 update on the product folder and dropped it into his file, now it appears much lower (erroneously) than the OPA1637. Frankly, afraid to check the Zol and Aol in this THS4561 model update, with the noise so far off, I will have to stick with the 2018 model for this next AX article and not waste time on this update,
here is that file where you have to reverse the supplies to use the new THS4561 model,
Audio-FDA_comparizon Zt with 2020 THS4561 model.TSC
Here is the input voltage noise sim for just the THS4561 2020 model, the 1/f corner is correct, but the flatband is way low from the PDS 4nV
And then the input current noise, this is way low on both flatband and 1/f if the PDS plot is correct,