Other Parts Discussed in Thread: TLV9052, TLV9001
Hi,
I have a simple Tina TI simulation with the LMV652 and observed that unless I apply a 5V supply voltage I don't see a full 3V swing on my output, the simulation clips at about 2.4V if I use my as designed 3.3V supply. The datasheet shows it should achieve within 90mV of the 3.3V rail at 3.3V and 25 deg C, figure 10&12. Is the simulation file incorrect or am I misinterpreting the datasheet in some way?
If my simulation is working correctly, could you please recommend a pin compatible (8 pin pkg dual ) that is rail to rail @ 3.3V? Low cost,general purpose, low power but ultra low power is not a requirement. The applications in this design are voltage measurement and temperature measurement, low frequency measurement of slow changing values.
ThanksPBIM V-Sense RPP.TSC