Other Parts Discussed in Thread: LM393
Please answer the following two questions.
①. Please tell me the input impedance and variation of the IN + / IN- terminals.
②. If the input voltage of the IN + / IN- pins is the same (when the Input Offset Voltage is less than 1 mV), will the OUT pin be a LOW output?