Other Parts Discussed in Thread: TPS61030, BQ24650, , TLV3012, TPS3700EVM-114
Hello,
I have recently purchased the TLV 3401 to ensure my 3.7 V 6000mah battery does not overdischarge by adding a low battery cutoff and release at 3.2 V and 3.3 V respectively to disable my loads.
Here is the schematic of my entire design:
Schematic_Final base model_2020-10-28_12-38-22.pdf
My solution looks at disabling voltage coming into pin 8 of the TPS61030 converters (U4 and U8) by attaching a comparator at the VBat output of my BQ24650 charger. How would I implement a noninverting comparator with hysteresis with the use of the TLV3401 for my battery??
I have attached a simpler diagram of my configuration: ( Please disregard the 3V trinket. The MCU being used will be an arduino nano powered by one of my TPS61030 boost converters)