Other Parts Discussed in Thread: OPA810
Hi,
I have a rather general query regarding offset voltage and bias/offset current specifications, given in datasheets. But for reference I've mentioned OPA837.
I was doing some error analysis on a circuit, containing couple of op-amps and few other stuffs, using propagation of uncertainty principle. However, I'm somewhat confused about the nominal value consideration of the above parameters (offset voltage and bias/offset current of the op-amps). I understand that the typical values, given in datasheet, correspond to the 1 sigma value. However, is it appropriate to assume these parameters as zero mean random variables?
The question I ask because typical schematics often show these variables have zero mean and normal distribution. However, in some recent datasheets (like OPA837), the offset voltage or offset current distributions (histograms) do not have zero mean. Intuitively, considering the mean as the most-likely value of a random variable, is it not true that zero offset voltage or current is unlikely (due to device mismatch)? Thus, choosing zero-mean could be contradictory, I feel. As a result, what should be the correct assumption of the the mean (and standard deviation from the mean) of these variables?
Looking forward to hearing from you.