Hello,
I am working on a design that also includes an LMV761 part, powered by a 3.3V (and the SD pin tied to the same potential). On the non-inverting input I have a DC voltage that comes from the output of an opamp and on the inverting one I have a reference triangle signal (generated in a microcontroller), rising from 0V, no offset. I did some tests with this circuit and found out jitter on the output of the comparator for a certain frequency of the triangle - 2.24 kHz. Also checked with some other higher frequencies and jitter disappeared.
Might useful to mention that Vdd is decoupled by 10 uF parallel with 100 nF.
What may be happening here?
Many thanks in advance for any suggestions, ideas!
Matei