This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV393: Out of spec performance (possibly fake part)

Part Number: LMV393

Just wanting to double check I''m not going mad. The datasheet shows that a 5v Vdd, a 140mV ref and a signal going up and below from 0 to 500mV is well within input-mode offset and overdrive for the slow frequency, but the output is always driven to a 700mV value (15k pull up to Vdd). I purchased these from lcsc.com and while they're usually good at ensuring brand name parts are genuine I do wonder if these aren't.

Tried 5 pieces now with the same outcome.