This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV07: Plans for a smaller package version?

Part Number: TLV07
Other Parts Discussed in Thread: OPA196

Are there plans to put TLV07 in a smaller package?  Seems like it is only available in SOIC-8 at the moment.

Thanks!

-Steve

  • Hi Steve,

    Indeed, the SOIC-8 is the only package the TLV07 is currently offered in. I have not seen any plans to offer it in any other package, but then again Applications Engineering is not always fully aware of what Marketing Engineering has planned.

    Even if Marketing does have something in the works announcements are made through the Marketing channels and not on the e2e. Let me check with Marketing Engineering and see if they have any information about you question that I can share.

    Regards, Thomas

    Precision Amplifiers Applications Engineering 

  • Thanks, feel free to email me internally if you like.  -Steve

  • Hi Steve

    Unfortunately, there are no plans for smaller packages on this one.

    We do, however, offer the OPA196 with the same DC offset in a SOT-23.

    The OPA196 is a CMOS amplifier, consumes less power and a has a lower noise floor.

    Let me know what you think of it?

    Soufiane