Other Parts Discussed in Thread: INA214, INA240
Related to my former post here:
https://e2e.ti.com/support/amplifiers/f/14/t/930415
The INA212 in our system is drawing 5mW - 6mW. I have confirmed this is not being drawn through VDD, but looks to be sunk through the IN+ / IN- Pins. Can you provide me with any input structures (caps, etc) that could cause this? The inputs are PWM signals with a typical carrier frequency around 300kHz - 400kHz. I suspect there is input capacitance in the INA212 that could be causing the current drain at these frequencies.
I have experimented with floating the device ground and VDD, but while the power draw can be improved slightly, it does not go away.
Even stranger, I have experimented with different PWM frequencies, and note that there seems to be a small window where power consumption is acceptable (400uA @ ~200kHz), but values above or below seem to increase back to the 6mW level.
Please also note that we are not using this opamp at these frequencies under normal circumstances. The INA212 in our system is used to take a periodic measurement (These 400kHz are disabled at this time), but when the periodic measurement is not taking place, the IN+ / IN- pins are exposed to these frequencies (with VDD grounded).
Any help you can offer would be greatly appreciated.
Thanks,
Andrew