This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2991: Transformer control

Part Number: OPA2991


Hello

Provide case details or comments:

Max. frequency of use sinus 10Khz 7.07Veff max. output current 30mA
This OP amp can drive a transformer type load?
What are the protections of uses ?

Case used OPA2991IDGKR in VSSOP
You can also propose me another reference but in the same type of case.
Thank you for your help
Best regards