hi,
we are looking for max Vos at max Vcm.
do we have such characterization data?
thanks
KR
Vincenzo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
we are looking for max Vos at max Vcm.
do we have such characterization data?
thanks
KR
Vincenzo
Hello Vincenzo,
Using full temperature max Vos and min CMRR,
At mid-rail and temperature Vos is +/-5mV and 5.5V minimum CMRR is 63dB. That is 0.707mV/V
From a 5.5V mid rail which is 2.75V to max VCM which is 5.5V - 1V = 4.5V makes a difference of 1.75V
So add another 1.75V * 0.707mV/V = 1.24mV
Final Vos maximum is +/-6.24mV
That only assumes CMRR response is first order (linear)