Other Parts Discussed in Thread: TLE2062M, TLC2252M, TLC2262AM, OPA2171-EP
Using a +/- 9V Supply, what is the achievable maximum voltage swing?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Using a +/- 9V Supply, what is the achievable maximum voltage swing?
Hello Christian,
With the 39 pages of redundant electrical characteristics it is no wonder that this would be a question.
The output voltage relative to the power rails will be based on the output current (little change with VCC value). For example the typical VOM+ for 10k load and +/-5V VCC is 3.7V (so that is an example of a 370uA output current with a result of VCC+ - 1.3V. So a 370uA output current at +/-9V would be 9V - 1.3V = 7.7V
With two VCC values, and two load values that gives 4 output currents that are specified in the data sheet. Is the application load current near any of the data sheet currents?
If the question is based on a worry about too much output swing, then that would require a completely different answer.
Hi Ronald,
Thank you for your response. The customer like the current consumption, footpint, temp range, high input impedance and J-FET input of TLE2062M, Do we have a similar device that can operate at a voltage range of at least +/- 9VDC with rail to rail output?
Regards,
Danilo
Danilo,
There are zero results for that search. If I lower supply to +/-8V then two results are found. TLC2262AM, TLC2252M. CDIP8
If I include all packages, then OPA2171-EP would work.