Other Parts Discussed in Thread: TLV379
We use the TLC27L2 in a product in which it is powered by a single 2v supply (below the recommended 3v lower limit for the "C" suffix part).
The part is used as a (dual) photodetector and log amplifier (log transimpedance amplifier) .
The PCB is tested with simulated photocurrents ranging from 2.5 microamps down to 2.5 nanoamps, checking for a ~60 mV output change per decade of current change.
For about 5% of the PCBs, when the current gets below 25 nanoamps the output voltage change per decade goes up, by far more than would be expected if the op amp bias current were only 60 pA (at room temperature). If the op amp is swapped out the PCB passes the test.
It doesn't appear to be a problem of leakage on the PCB - the PCB is laid out with guard rings and carefully cleaned prior to test. Re-cleaning failed PCBs multiple times doesn't solve the problem, but changing the op amp does.
Question: What is causing this problem? If the supply voltage is too low, does the bias current increase? Or is there something else going on?
Thank you for your assistance.