Hi,
I'd like to know how to calculate the two-stage OP amp's noise voltage.
Whether it is accurate that add up each stage's noise voltage.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'd like to know how to calculate the two-stage OP amp's noise voltage.
Whether it is accurate that add up each stage's noise voltage.
Thanks.
Hi Eric,
yes, if you keep in mind that the noise of stage 1 is amplified by stage 2 and that noise is added geometrically (sum over the squares...).
It turns out that when choosing a high gain in the first stage, the noise of the following stages can become negligible. For instance: SQRT ( 1^2 + 0.3^2) = 1.04 which equals an increase of noise of only 0.3dB :-)
Can you post a schematic with concrete component values?
Kai