Other Parts Discussed in Thread: TEST
Hello,
I have a question about INA290A4Q(200V/V).As shown in the figure,I add a RC filter(R=100ohm,C=1uF) for the output,and then to the DSP(280049).But the sample voltage between iL_sam and iL_samf is different.iL_sam is about 200mV,but iL_samf is about 500mV.The detected currrent is about 1A ,and the shunt resistor is 1mΩ .
Best Regards.