This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA237-Q1: Writing/Reading consecutive several registers w/o pointer set

Part Number: INA237-Q1

Hi all,

Is it possible for the master connected to INA237-Q1 to read/write two or several consecutive registers at once like the figure below? Or should register pointer set command be sent when any register read/write finished if you want to read/write another continuous registers?

Regards,
RYO

  • Hello RYO,

    This is not possible for the INA237-Q1. This device does not auto increment the register pointer to allow repeated reads from the same register without a write.  If you want to read/write to a different register they you'll need to write to the register address pointer first.