Other Parts Discussed in Thread: DRV595, , INA260, INA228, INA229, INA237, INA238, INA239
Hi-
We are driving two TECs in series with a DRV595, highest Vbus will be 24V, largest current will be 4A. We'd like to use the INA226 to sense the current in both directions for when the TECs are heating or cooling. There is a 10uH inductor in series in each leg with OUTP and OUTN to the TECs. Wondering if you have a suggestion on where to put Rsense, and what connections to make to the INA226 for Vbus sensing, as the polarity of the voltage will switch with the current? Should Rsense be from pins 22 and 28 of the DRV595 (grounds for the outputs)? In this case, we wouldn't be able to verify heating or cooling by the direction of the current...
If we can't read the Vbus, that is acceptable in this case. Should the Vbus input be tied to either Vss or Gnd, or NC?
Or perhaps we should go with something like the INA260 if we can't read the current direction?
Thank you