Other Parts Discussed in Thread: INA201, INA193, INA226, INA220
Hi team,
I have questions on BW of current sensor.
1. INA282 has 10kHz of BW, which is quite narrow when it's compared to other INA parts such as INA193 and INA201 (300kHz and 500kHz each). Does this mean INA282 would show much slower output response when it comes to Vsense (V+ - V-) transient?
2. I found current sensors with digital output type such as INA220 and INA226 (5.5kHz and 3.5kHz each) have much narrow BW than analog current sensors do. The digital processing time would be added as well, so I assume that the total response time would be so slow when it's compared to the case of analog current sensors like INA193 and INA201. Could you correct me if any misunderstanding?
- BW indicates not only frequency range that the internal opamp can pass but also the response speed from my understanding.