Other Parts Discussed in Thread: LM2904, , LM331
For one of my companies products, I've designed in the version that is GND referred. We primarily hook it up to a variable reluctance sensors or even avionic instrumentation that uses a generator to indicate tach. These are two wire deals. Some of them are GND referred, however trying to dig out of the avionic docs which wire is GND and which is signal is problematic. The aviation docs don't indicate this. They merely serve the purpose for the maintenance people to prove things are hooked up correctly. Unfortunately, if we choose the signal wire to be GND and the GND wire to be signal we have grounded a cockpit gauge - definitely a no-no. Therefore I am changing the design to use the differential version of the LM2904. While prototyping this I notice the output DC voltage appears to hunt after an input frequency step change. It exhibits the classic behavior of an underdamped servo loop whereby the initial change in the input F creates an overshoot on the output in V. Thereafter this rings out. I went back to observe the original single ended design - does the same thing. Increasing the value of the output cap that reduces ripple makes it the amplitude fluctuation worse and makes the the rate of the ring-out longer. Of course decreasing the cap increases the amplitude of the ripple which also not desirable.
Any suggenstions?