This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3201-Q1: Temperature curve

Part Number: TLV3201-Q1
Other Parts Discussed in Thread: TLV3201

Hi I have read the datasheet of TLV3201-Q1,

There has the curve of Output Voltage vs Output Current with full range temperature of 2.7V and 5.5V

but we are using 5V as the input voltage with tolerance ±1%,

so can TI offer the curve of Output Voltage vs Output Current with full range temperature of 5V±1%?

or the calculate between Vout with Temperature and Current

We are using as frequency oscillator, so the vout voltage will effect the RC time constant 

Thanks for apply.