Hi TI-team
My customer are using the INA240A2QDRQ1.
They have some question.
1.When they searched the E2E forum because they wanted to know the values of internal resistances A to F, the resistance was described at the following URL.
A = 500 kohm
B = 25 kohm
C = 25 kohm
D = 475 kohm
E = 50 kohm
F = 50 kohm
Are these TYPs ?
They wants to know the TYP and MIN values.
Could you tell me ?
2.Which is the polarity of the internal amplifier input stage, n or p ?
3.What is the leak current from IN± to GND and from IN± to OUT of the internal amp during sleep ?
Best Regards,
Koji Hayashi