Hi there,
I have questions about INA230 alert below;
1. from data sheet, "If multiple alert functions are enabled, the selected function in the highest significant bit position takes priority and responds to the Alert Limit register value. For example, if the SOL and the SUL are both selected, the ALERT pin asserts when the Shunt Voltage Over Limit register exceeds the value in the Alert Limit register". Does it say only SOL will send alert? SUL will not trigger, even SUL is set at enable? Only 1 item can be monitored in case 2 or more items are set, right?
2. In Alert register (07H), how do I set the threshold value? Does it support over current feature? example: bus over voltage, Vin = 12V normally, 13.2V is OVP target. 13.2V or 1.2V should be used in Alert register? And only 1 protection can be stored, right?