I have an application where I need to measure differentially a voltage that is nominally between 5 and 25 volts. However, under overload conditions, the input can go as high as 72 volts. The INA146 looks like it can handle this with a unipolar 12 volt supply. My question is about the isolation of the input pins. The SOIC package has pins on .050 inch centers while the insulation distance is much smaller. What do you recommend to handle this? I could conformal coat these components if absolutely necessary. Thanks.