Other Parts Discussed in Thread: THS4524, ADS1274, OPA1632, THS4521, ADS1278
Hello,
I have to design a driver for the AD converter ADS1274 to get maximum performance. In the datasheet of the ADC the amplifier THS4524 is recommended. The obvious advantage is the lower price and form-factor, because four amps are in one case. However, the evaluation kit contains 4x OPA1632.
Does the OPA1632 perform better than the THS4524 in this case (my signals are mixed sine waves in the frequency range of 1kHz-20 kHz, linearity is important)?
What else do I have to consider when I have to decide between these two amplifiers?
Thanks a lot and best regards,
Markus.