This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Well Eric,
The open loop transresistance gets into the closed loop gain as a LG/(LG+1) term where the LG is approx. that transresistance divided by the feedback R. Very small part of the overall gain drift.
That said,the datasheet min is a worst case designer simulation using full process variation models. There is however a limited number of devices run through full ATE overtemp at release - this would include everything shown as an "A" spec in the far right column - including transresistance - that data exists somewhere, perhaps someone can pull it out.
Hi Michael,
Thanks for the response, I am definitely interested in seeing the data measured for transresistance to get the "A" specification rating. Can someone at TI provide this information to me?
Thanks,
Eric
Also, thanks for the comment Kai. Yes, I understand your point having an amplifier with much larger transresistance or open loop gain where it is not a design limiting factor is normally the approach taken. Unfortunately figure 6 does not provide enough information for me, I was hoping to see an actual dataset or get a number for gain drift per C.
Hello Eric,
Unfortunately, we do not have data for specifically gain drift per C, but I can share additional frequency response varying with temperature data offline. I also have some data on release (as Michael mentioned) for open-loop transimpedance gain numbers at various temperatures that I can share as well offline.
Thank you,
Sima
Thanks Sima, yes please share the information with me. I notice on the datasheet it specifies the test conditions are RL = 500 ohms and Vo = +/-10V, if you have any data when RL is changed or Vo is outside of the +/-10V range please let me know as well - Would you expect the transimpedance gain to change much as Vo gets closer to the supply rail?
Hello Eric,
Sorry for the late response, I do not have any additional data other than what is presented in the datasheet for variations in output voltage swing and load resistance. It does change a bit in the frequency response, check Figures 4, 5 (impedance load), and some of the pulse response vs output voltage figures.
Thank you,
Sima