Other Parts Discussed in Thread: LM124
Hi,
In the datasheet of the LM124AQML the output voltage swing is given at (V+)-1.5V in the features and further in the document is given at Voh 26V or 27V according to the load for V+=30V.
Can you say what value can I take for a worst case analysis in the following conditions
V+=12V or 15V, V-= GND, output current < 1mA
Datasheet reference : SNOSAE0K –AUGUST 2004–REVISED MARCH 2013
Regards
Matthieu