Other Parts Discussed in Thread: XTR305, , TIPD155
Dear TI Team
Our customers are requesting Vin vs Vout measurement data when using the XTR300 and XTR305 in voltage output mode.
(To understand the error of Vout with respect to Vin (how much error there is from the set output voltage))
For example, is it possible to use the XTR300EVM circuit and measure Vin vs Vout data under the following conditions?
(I hope you can see the device on both XTR300 and XTR305.)
・ Power supply voltage: ± 15V applied to V + and V- pins
・ Vin = -12V ~ 12V
・ Rset = 2.5kΩ
・ Rgain = 10kΩ
(If you have reference data for Vin vs Vout (Vout error) on XTR300 and XTR305, I would be grateful if you could.)
Best Regards,
Y.Ottey