Other Parts Discussed in Thread: INA199,
Hi
Please suggest products suitable for DDR Nvdimm
Which of these two is suitable for LMP8640 & INA199
common mode :12V
Rsense: 2m ohm
Iout: 4.2A
ADC: input 0~3v
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Based on the conditions you provided, either of these two can be used. However to help with overall evaluation, I made this side by side comparison.
Regards, Guang