Other Parts Discussed in Thread: TINA-TI
Hi,
I downloaded the PSpice model for LMH6703C from the TI website "snom578" and I added the model to the Allegro CIS library. I created a simple circuit to test the model, however, I received an error. Here is a snapshot of the circuit I built and the error:
"*Analysis directives:
.TRAN 0 1000ns 0
.OPTIONS ADVCONV
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*))
.INC "..\SCHEMATIC1.net"
**** INCLUDING SCHEMATIC1.net ****
* source LMH6703
V_V1 VCC_BAR 0 5Vdc
V_V2 VEE_BAR 0 -5Vdc
R_R5 0 N01272 1k TC=0,0
R_R6 0 N01078 1k TC=0,0
R_R7 0 N01099 1k TC=0,0
R_R8 0 N01094 1k TC=0,0
X_U1 N01272 N01078 VCC_BAR VEE_BAR N01094 N01099 LMH6703C
**** RESUMING LMH6703sim.cir ****
.END
ERROR(ORPSIM-15108): Subcircuit LMH6703C used by X_U1 is undefined"
Could you please help me fix this error?
Thanks,
Ahmad