Hello,
the datasheet states Vos=0.2mV typ. @ Ta=25°C and Vos=1mV max. @ Ta=-40...+125°C.
Does this mean an offset voltage of +/-0.2mV and +/-1mV, or +0.2mV/-0mV and +1mV/-0mV?
Regards, Oliver
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
the datasheet states Vos=0.2mV typ. @ Ta=25°C and Vos=1mV max. @ Ta=-40...+125°C.
Does this mean an offset voltage of +/-0.2mV and +/-1mV, or +0.2mV/-0mV and +1mV/-0mV?
Regards, Oliver
Thanks Kai for clarifying.
Oliver,
this was old nomenclature to only list one number but Kai is correct, it is +/-
Chuck