Other Parts Discussed in Thread: INA240, INA280, INA290, INA281
HI,
Looking at the INA191 datasheet in the Absolute Maximum ratings section, Note 3 states - (3) Input voltage at any pin may exceed the voltage shown if the current at that pin is limited to 5 mA.
In my application the current will be limited to 1mA. Greater than this will likely damage other components in the circuit.
Is it possible for the Common mode voltage to be even higher than 42V?
If 42V is the maximum under all conditions. Will the INA191 function properly over temperature (-40 to 85C) ?
Regards,
Roy