Other Parts Discussed in Thread: LM339
I am using the LP2901 quad comparator. There are some instances where the voltage on the V- input may reach 28V. This would not violate the 36V input maximum rating +/-36VDC differential voltage maximum rating. However, the VCC of my device is 9V. Will the comparator still function and output a low if this comparator momentarily hits 28V?
Thanks
Bradley Wynn
703-889-8640 x1041