Hi team,
Can I connect positive input V+ or negative input V- to ground directly when I use this device? Is there any risk if I use in this way.
Thanks for support!
Jayden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Can I connect positive input V+ or negative input V- to ground directly when I use this device? Is there any risk if I use in this way.
Thanks for support!
Jayden
There is danger only if the voltage at an input can become smaller than the voltage at the ground pin (absolute maximum rating: –0.3 V). This might happen with symmetric supplies that power up too late, or if there are very large (transient) currents in the ground trace between the input and ground pins.
Jayden,
Can you repeat the question more clearly?
Also check user guide, Design Guidelines for Devices with LM324/LM358 Cores