Hi,
I have a query on the changes made to the following parameters in the latest datasheet "SBOS538F" w.r.t. the previous revision of the datasheet "SBOS538E".
1. Input Offset Voltage vs Temp (dVos/dT): In datasheet SBOS538E, the parameter values were boldened to signify that the values are specified for the temp range of -40'C to +125'C. But in the latest datasheet SBOS538F, the format has been changed and the Test Conditions does not specify the full temp range. Does it mean that the Typ & Max values specified for the parameter are only applicable for Ta=+25'C? If so, is there any characteristic curve available which captures the "change in input offset voltage vs temp" for this device? Could you please confirm whether there is any change to the actual device due to which the electrical characteristics section has been updated?
Please see below snippets for reference.
2. Open-loop voltage gain (AOL): Similar case as mentioned above (please see snippets below)
Could you please confirm whether there is any change to the actual device due to which the electrical characteristics section has been updated?
Thanks
Vijay