Other Parts Discussed in Thread: TL331-EP
Team, Can you help with the below questions:
- Saturation Voltage of the output BJT
- The datasheet specifies it at 0.23, typ to 0.4, max at 8mA. Do you have data on what we should expect when operating at the 0.5mA to 1mA range? Would be nice if you had a plot of Vsat verses collector current.
- Input Common mode Clarification
- The typical specification is 13.8 at the upper end and -14.7 at the lower for +/-15V supply. Section 9.2.2.1 is somewhat confusing in its description of the input voltage ranges. In particular When IN- is higher that common mode and In+ is within… What about if it is lower than common mode, -14.9 or –VCC?
In the past I’ve always used (IN- + IN+)/2 is the common mode voltage and as long as that voltage is within the common mode range of the part you would be good to go (basically if both inputs don’t exceed the common mode range at the same time). I want to apply a reference to the non-inverting input and sense a voltage that will start at ground and ramp up with VCC- being at ground. I should be good with this design.
It’s been a while since I’ve used a comparator that did not include VCC- in the common mode range and I would rather check.