Hi Team,
Concering with the AMPs and load resistor, i had a few queries below:
1.The output terminal of op amp is connected with resistance load, the load resistance value is different, the output voltage range is different, but the open-loop output impedance of op amp tl082 is 125 Ω, the influence of internal resistance of op amp should not be so great. The picture on tl082 specification shows that the influence of load resistance is still very large (larger than the voltage difference caused by the internal resistance of OP AMP (I calculate it by 128 + 64 Ω) and the output load resistance). The output voltage of the op amp is related to the load resistance. What is the reason?
2.DSP_ADC The input model of ADC is sample and hold type. There is no pull-down load resistor in DSP. I have seen most Voltage Feedback Op Amp outputs with load resistor, but it seems that some op amp output signals are directly sent to DSP_ ADC pin, no load resistance. So the question is: when does the load resistor of the op amp need to be added or not? Is the load resistor applied to provide a bias current path to the inverting input of the op amp?